Presses
We offer on-site electrical control repair on presses!
Galco's expert field service technicians can service and repair electrical control components that control your press fast. Our technicians have long time experience with all kinds of industrial machinery, and are factory trained with quality solutions. Our fast response time minimizes your downtime. Our technicians also have a parts advantage with access to Galco's millions of in stock parts!
What we'll do:
- Contact you: We'll contact you to schedule your field service appointment at a time that is best for you.
- Contact you: We'll contact you to schedule your field service appointment at a time that is best for you.
- Get your Approval: We'll ask for your approval to proceed.
- Dispatch the Technician to Your Location: The technician will then be dispatched to your location to service your application.
- Troubleshoot your Machine: Upon arrival the technician will troubleshoot your application.
- Offer a Solution: After troubleshooting we will work for a solution to your problem. The technician will attempt repairing your application or we can offer you new control units.*
- Quality Follow-up: Once service on your application is complete you will receive a follow-up phone call for a quality check.
Call to schedule your on-site service today!
800-575-5562
What is a Press?
A press is a machine that is used to shape, bend, cut, or fold materials such as plastic, metal, paper, or wood. The material rests or is fastened to the bolster while the die moves downward into the material causing the bend or cut into the desired shape.
Types of Presses
- Brake Press: Brake presses use hydraulics to move a wedge down into the work pressing the metal into open space below the work. This causes a bend in the metal at a certain degree of angle.
- Punch Press: Punch presses are used to create holes in materials such as metal, wood, or plastics. The material usually passes through the press, is secured while it is being formed or cut, and then moves on for more material to pass.
- Stamp Press: Stamping presses are used for cutting and shaping metal. The metal or some other material is fastened to the bolster while the die presses the secured metal creating the desired size and shape of metal.
- Printing Press: Printing presses are used to create text and images on paper. The paper passes through the machine while the ink is rolled or pressed onto the sheets of paper by applying pressure.
Manufacturers
Some press manufacturers include:
- Promess
- Alfra
- Silcon
- Megafab
- Beckwood
- Bruck
- Cantec
- Bruderer
- Minster
- Pivatic
- Simpac
- Triform
- Rotatek
- Hemingstone
- Maflex
Industries
Presses are commonly utilized in these industries:
- Machining
- Fabrication
- Metal Processing
- Paper
- Printing
Products Used in Press Applications
These products can be found controlling presses:
- AC Drives
- DC Drives
- Servo Drives
- Light Curtains
- Monitors
- HMIs
- PLCs
Common Problems & Failures
Common points of failure:
- Fusing
- connections and wiring
- AC or DC drives
- Phase control
- Switches and push buttons
- Proximity and limit switches
- Feedback devices
- Overloads
- Relays and contactors
- PLCs
- Fans
*Based on circumstance, not all machines can be repaired under our capabilities and warranties are not offered.