Skip to content

How to Source Process Control Components

Process-control systems depend on the right components arriving at the right time. A delayed PLC, sensor, variable frequency drive, relay, power supply, or communication module can hold up a new project or extend downtime during an equipment failure.

Sourcing process-control components involves more than searching for a part number or comparing prices. You also need to consider technical compatibility, product availability, lead times, documentation, support, repair options, and the supplier’s ability to respond when requirements change.

Whether you are maintaining an existing system, assembling a control panel, replacing an obsolete component, or purchasing parts for a new project, the following steps can help you make a more informed sourcing decision.

Define the Application Requirements

Before contacting a supplier, document what the component must do within the system.

Useful application details may include:

    • Manufacturer and complete part number
    • Voltage, current, power, or horsepower requirements
    • Number and type of inputs and outputs
    • Communication protocol
    • Environmental conditions
    • Required certifications or approvals
    • Panel space and mounting requirements
    • Quantity and required delivery date
    • Whether an exact replacement is required
    • Whether a repair, cross-reference, or upgrade is acceptable

For replacement components, include the original product’s series, revision, firmware, and installed options whenever possible. Clear photos of the nameplate, terminals, connectors, and mounting arrangement can also help a supplier identify the correct product.

The more complete the information, the easier it is to avoid specification mismatches, incorrect orders, and unnecessary delays.

Verify Component Compatibility

Products that look similar or share several specifications are not necessarily interchangeable. Compatibility should be reviewed across the complete application.

PLCs and I/O Modules

When sourcing PLCs, processors, and I/O modules, confirm:

    • Controller family and platform
    • Rack, chassis, or backplane compatibility
    • I/O type and channel count
    • Firmware and programming-software requirements
    • Terminal block or wiring-arm compatibility
    • Communication and addressing requirements

A newer module may require a firmware update, software conversion, different terminal block, or changes to the existing program.

HMIs

For human machine interfaces, evaluate:

    • Screen size and panel cutout
    • Resolution and touchscreen type
    • Supported PLC communication drivers
    • Programming software
    • Available project files
    • Communication ports
    • Environmental rating

Replacing an obsolete HMI may require project conversion or redevelopment if the original application file is unavailable.

Sensors and Transmitters

For sensors, pressure transmitters, temperature devices, flow instruments, and level controls, check:

    • Measurement or sensing range
    • Accuracy
    • Supply voltage
    • PNP, NPN, analog, or digital output
    • Connector or cable type
    • Process connection
    • Response time
    • Environmental rating

A sensor with the same housing may still use a different output configuration or sensing range.

Variable Frequency Drives

Do not select a replacement VFD based only on horsepower. Review:

    • Input voltage and phase
    • Motor full-load current
    • Continuous output current
    • Overload rating
    • Motor type and control method
    • Communication requirements
    • Braking or feedback options
    • Enclosure rating

Drive parameters and control wiring may also need to be transferred or reconfigured during replacement.

Evaluate Availability and Lead Times

Availability can affect both project schedules and maintenance response.

Ask whether the component is:

    • In stock
    • Available from the manufacturer
    • Subject to an extended lead time
    • Discontinued or approaching obsolescence
    • Available through an alternative manufacturer
    • Repairable if a replacement cannot be sourced

For planned projects, evaluate lead times early enough to identify potential shortages before panel assembly or installation begins.

For MRO applications, consider maintaining spares for components that are critical to production, difficult to source, or installed across multiple machines. Spare-parts planning can reduce dependence on emergency sourcing when equipment fails.

Consider the Appropriate Sourcing Path

The best sourcing option depends on the component, system age, urgency, and long-term plans for the equipment.

Exact Replacement

An exact replacement generally involves the least system modification, but the complete part number, series, revision, firmware, and options should still be verified.

Manufacturer Successor

The original manufacturer may recommend a newer product as the replacement or migration path. A successor may require adapters, new software, wiring changes, or parameter conversion.

Cross-Referenced Alternative

When the original component is unavailable, another product may be able to perform the required function. Cross-referenced alternatives should be treated as candidates until electrical, mechanical, communication, software, environmental, and safety requirements are verified.

Repair

Repair may be practical when the component is obsolete, difficult to replace, or configured specifically for the application. PLCs, VFDs, HMIs, servo drives, circuit boards, and power supplies may be repairable depending on their condition and failure mode.

Retrofit or Upgrade

A retrofit may be the better long-term option when replacement inventory is limited, several parts within the system are obsolete, or the existing platform no longer supports operational requirements.

Evaluate the Supplier, Not Just the Product

A supplier’s capabilities can affect how quickly and accurately you complete a sourcing project.

Inventory and Shipping

Determine whether the supplier maintains its own inventory or relies primarily on manufacturer fulfillment. Also review available shipping options and expected processing times.

Technical Support

Access to knowledgeable technical support can help with:

    • Product selection
    • Cross-referencing
    • Compatibility questions
    • Application requirements
    • Obsolete-part replacement
    • Troubleshooting
    • Repair-versus-replace decisions

This is particularly important for system integrators, panel builders, OEMs, and MRO teams working with multiple product categories or legacy systems.

Multi-Brand Product Access

Many process-control systems use products from several manufacturers. Working with a distributor that carries multiple brands can simplify purchasing, reduce the number of suppliers involved, and make it easier to source a complete bill of materials.

Documentation

Verify that product manuals, data sheets, drawings, certificates, and technical specifications are available. System integrators and OEMs may also need dimensional drawings, CAD files, and approval documentation during panel or machine design.

Repair and Legacy Support

Suppliers with industrial electronics repair capabilities may provide another path when replacements are unavailable or when modifying the machine would be costly.

Plan Bulk and Ongoing Purchases Carefully

Bulk purchasing requires additional coordination beyond ordering a single component.

Before placing a large order, confirm:

    • Quantity pricing
    • Current inventory
    • Manufacturer lead times
    • Scheduled-release options
    • Partial-shipment policies
    • Product lifecycle status
    • Return restrictions
    • Warranty terms
    • Documentation requirements

For recurring requirements, share anticipated quantities and delivery schedules with the supplier. Advance planning may help identify availability risks and reduce the need for last-minute substitutions.

Blanket orders or scheduled releases may also help balance product availability with internal inventory-management goals.

Document Approved Components and Alternatives

Once a product has been selected and verified, document it for future purchasing and maintenance.

Record:

    • Manufacturer and complete part number
    • Approved substitute or successor
    • Required series or firmware
    • Configuration requirements
    • Supplier information
    • Lead time
    • Installation notes
    • Drawings and manuals
    • Backup-file location
    • Date of approval

Updating bills of materials, schematics, CMMS records, and approved-parts lists can make future sourcing faster and reduce the risk of ordering an incompatible product.

How Galco Supports Process-Control Component Sourcing

Galco helps maintenance teams, engineers, system integrators, panel builders, OEMs, and industrial resellers source automation and control products for new systems, replacements, repairs, and upgrades.

Support may include:

    • Product selection assistance
    • Multi-brand component sourcing
    • Cross-reference support
    • Obsolete and hard-to-find component assistance
    • Industrial electronics repair
    • Technical product information
    • Bulk-order and project support

Galco supplies process-control and industrial automation products including PLCs, HMIs, sensors, transmitters, variable frequency drives, relays, contactors, power supplies, communication products, and panel components.

Need help sourcing process-control components?

Send Galco the manufacturer, complete part number, quantity, required delivery date, and available application information. Call 800-575-5562 or contact Galco to discuss product availability, replacement, cross-reference, and repair options.

Frequently Asked Questions

What should you consider when sourcing process-control components?

Consider compatibility, availability, lead time, technical support, documentation, lifecycle status, repair options, and the supplier’s ability to support the complete application.

How can system integrators simplify component sourcing?

System integrators can work with suppliers that offer multi-brand product access, technical guidance, documentation, cross-referencing, and support for complete bills of materials.

What should MRO teams look for in a component supplier?

MRO teams should prioritize inventory availability, response time, obsolete-part support, repair capabilities, technical assistance, and shipping options.

Why is technical support important when sourcing automation components?

Technical support can help verify specifications, identify replacement options, prevent ordering errors, and address compatibility issues involving hardware, software, communication, and installation requirements.

When should an obsolete component be repaired rather than replaced?

Repair may be appropriate when a replacement is unavailable, the system is difficult to modify, or the original component contains application-specific configuration. The decision should consider repairability, downtime, machine life, and future support.