Space-focused manufacturing and testing often depend on controlled movement, pressure, and force. Production cells, test stands, fixtures, handling equipment, and facility support systems may all use hydraulic or pneumatic components to clamp, lift, position, actuate, regulate, or monitor equipment.
That makes hydraulic and pneumatic support an important part of space economy infrastructure. Valves, cylinders, regulators, filters, fittings, tubing, hoses, gauges, pressure switches, transducers, and manifolds help teams manage air and fluid systems that keep equipment operating properly.
For manufacturers, engineers, integrators, and maintenance teams, the goal is not just to move air or fluid through a system. The goal is to create controlled, reliable, and serviceable assemblies that support repeatable production and testing.
Space economy operations may include satellite manufacturing, component assembly, environmental testing, cleanroom support, test equipment, and ground infrastructure. In many of these applications, equipment needs controlled actuation or regulated pressure to perform correctly.
Pneumatic systems may be used for clamps, slides, grippers, indexing equipment, valve actuation, fixtures, or light-duty motion. Hydraulic systems may support applications that require higher force, stable movement, lifting, pressing, or controlled positioning.
When these systems are not properly maintained, small issues can become larger disruptions. A leaking fitting, clogged filter, pressure drop, damaged hose, or sticking valve can affect equipment movement, process consistency, and test reliability.
The right components help teams maintain pressure, control movement, reduce leaks, and identify problems earlier.
Pneumatic systems use compressed air to create motion and control equipment functions. They are often used when teams need fast, repeatable movement without the force requirements of a hydraulic system.
In space-focused manufacturing and testing environments, pneumatic components may support fixture movement, part handling, clamping, indexing, door actuation, or test stand functions. Common components include cylinders, valves, regulators, filters, lubricators, tubing, fittings, silencers, and manifolds.
Regulators help maintain proper air pressure. Filters help remove contaminants from compressed air. Valves control when air moves through the system. Cylinders and actuators convert that air pressure into motion.
When selected and maintained correctly, pneumatic assemblies can help equipment move consistently and support more dependable production or test sequences.
Hydraulic systems are used when an application needs greater force, smoother load handling, or more stable movement. These systems may support lifting platforms, positioning equipment, presses, clamping systems, test fixtures, or support machinery.
Hydraulic assemblies may include pumps, valves, cylinders, hoses, fittings, filters, gauges, reservoirs, pressure switches, and transducers. Each component plays a role in helping the system maintain pressure, control movement, and protect equipment.
Hydraulic reliability depends heavily on clean fluid, proper pressure, secure connections, and component condition. Contamination, leaks, worn seals, blocked filters, or pressure instability can reduce system performance and create maintenance issues.
For demanding production and test environments, hydraulic components need to be selected for the load, duty cycle, pressure range, environment, and service requirements of the application.
Valves and regulators are key to controlled hydraulic and pneumatic operation. They help determine where air or fluid goes, when it moves, and how much pressure is available.
Directional control valves help start, stop, or redirect flow. Solenoid valves allow electrical signals to control pneumatic or hydraulic functions. Pressure regulators help maintain consistent air pressure for pneumatic devices. Flow controls help adjust actuator speed or manage movement.
In test stands and production cells, these components help equipment behave predictably. A clamp needs to close with enough force. A cylinder needs to extend at the right speed. A fixture needs to move only when the system is ready.
Reliable valves and regulators help create smoother operation and reduce the chance of unexpected movement or inconsistent equipment response.
Hydraulic and pneumatic systems need pressure visibility. Without it, teams may not know whether a system is operating at the right level until performance changes or equipment faults.
Pressure gauges provide local visual confirmation. Pressure switches can trigger a signal when pressure reaches or falls below a set point. Pressure transducers provide continuous measurement that can be sent to a controller, display, or monitoring system.
These products can help teams identify leaks, blocked lines, supply issues, failing components, or pressure changes that affect equipment performance. In testing and production environments, pressure information can be especially useful when a fixture, actuator, clamp, or process function depends on consistent force.
Better pressure visibility supports faster troubleshooting and more informed maintenance.
Fluid power and pneumatic systems depend on the quality of their connections and media. Filters, fittings, tubing, and hoses may seem like supporting components, but they play a major role in system reliability.
Filters help protect valves, cylinders, regulators, and other components from contamination. Fittings and connectors help maintain secure, leak-resistant connections. Tubing and hoses route air or fluid through the system and need to be selected for pressure, flexibility, environment, and compatibility.
Leaks, restrictions, contamination, or damaged lines can reduce performance and create service issues. A strong maintenance strategy should include regular inspection of tubing, hoses, fittings, filters, and visible connection points.
These components help keep the system clean, connected, and dependable.
Reliable hydraulic and pneumatic assemblies depend on components that control pressure, movement, flow, and system condition.
A strong system may include:
• Pneumatic cylinders and actuators for controlled movement
• Hydraulic cylinders for force, lifting, clamping, or positioning
• Directional valves and solenoid valves for flow control
• Regulators and flow controls for pressure and speed adjustment
• Filters for air and fluid cleanliness
• Fittings, tubing, and hoses for secure connections
• Pressure gauges for local system visibility
• Pressure switches and transducers for monitoring and alerts
• Manifolds for organized air or fluid distribution
Each component helps support controlled actuation, pressure stability, cleaner operation, and more serviceable equipment.
Call 800-575-5562 today. Our solutions experts are ready to assist you.