Skip to content

How to Cross-Reference Obsolete Automation Parts

Industrial control cabinet with modern and legacy automation components beside the text, “How to Cross-Reference Obsolete Automation Parts.”

Industrial facilities often rely on automation components that have been in service for years. When a PLC module, variable frequency drive (VFD), HMI, sensor, relay, circuit board, or power supply becomes obsolete, finding the right replacement can quickly become a downtime issue.

To cross-reference an obsolete automation part, start by identifying the exact manufacturer, complete part number, series or revision, firmware, and installed options. Then compare the original component’s electrical, mechanical, communication, software, environmental, and application requirements against available replacement options.

The result may be an exact replacement, an updated manufacturer successor, a functional alternative, a repair, or a system upgrade.

A cross-reference should always be treated as a candidate replacement until compatibility is verified. Similar specifications or physical dimensions do not necessarily mean that two parts are interchangeable.

Why Obsolete Automation Parts Are Difficult to Replace

Industrial automation manufacturers regularly discontinue older product lines and introduce updated platforms. Even when a newer component appears similar, it may not support the existing hardware, software, wiring, or communication architecture.

For example:

    • A newer PLC module may require a different rack, chassis, terminal block, firmware version, or programming package.
    • A replacement VFD may match the motor horsepower but have different output-current, overload, control, or communication requirements.
    • A replacement HMI may require a different panel cutout, programming application, or PLC communication driver.
    • A sensor may have the same housing but use a different voltage, output type, connector, or sensing range.

That is why cross-referencing should be handled as a technical review, not simply a part-number search.

Step 1: Collect the Complete Part Information

Before requesting a cross-reference, gather as much information as possible about the original component.

Useful details include:

    • Manufacturer name
    • Complete part or catalog number
    • Model or product family
    • Series, revision, or hardware version
    • Firmware version, when applicable
    • Voltage, current, horsepower, power, or I/O ratings
    • Communication protocol and installed option cards
    • Photos of the nameplate, terminals, connectors, and mounting arrangement
    • Machine, panel, rack, chassis, or slot information
    • Failure symptoms or error codes
    • Quantity needed and urgency
    • Whether repair or upgrade options are acceptable

Pay close attention to prefixes and suffixes. A small difference in a catalog number may identify a different voltage, enclosure, communication interface, feedback option, coating, or I/O configuration.

Original documentation can also help. Review schematics, wiring diagrams, bills of materials, maintenance records, equipment manuals, PLC programs, HMI applications, and drive parameter files when available.

Before removing a component that still powers up, back up any available configuration data. This may include PLC logic, HMI applications, VFD parameters, servo settings, network addresses, recipes, or safety-controller projects.

Step 2: Identify the Best Replacement Path

Once the original part and its application are understood, determine which replacement path makes the most sense.

Exact Replacement

An exact replacement uses the same complete part number, with the required series, revision, firmware, and options verified.

This is often the lowest-change option, but the same base model number does not always mean that two units are equivalent.

Manufacturer Successor

A manufacturer successor is an updated product identified by the original manufacturer as the replacement or migration path.

A successor may still require adapters, software conversion, parameter migration, new terminal blocks, or wiring changes. Always review the manufacturer’s migration documentation.

Functional Alternative

A functional alternative is a different product line or manufacturer that may perform the same required function.

This option may require additional engineering, rewiring, reprogramming, network changes, or renewed application testing. Similar ratings alone do not establish compatibility.

Repair

Repair may be practical when the machine is difficult to modify, the component contains application-specific configuration, or replacement inventory is limited.

PLCs, VFDs, HMIs, servo controls, circuit boards, and power supplies may be repairable depending on their condition and failure mode.

Retrofit or Upgrade

A retrofit modifies the machine or control system to use newer technology.

This may be the better long-term option when repair and replacement inventory are becoming unreliable or when multiple obsolete components create continuing lifecycle risk.

Step 3: Verify Compatibility

Before installing a replacement, confirm that it meets the complete application requirements.

Electrical Requirements

Check:

    • Input and output voltage
    • Current and power capacity
    • AC or DC operation
    • Input and output type
    • Load characteristics
    • Grounding and isolation
    • Overload requirements

For VFDs, compare the motor full-load current and required overload rating, not just horsepower.

Communication and Software

Confirm that the replacement supports the required communication network or interface, such as EtherNet/IP, Modbus, PROFIBUS, PROFINET, DeviceNet, serial communication, or IO-Link.

Also verify:

    • Network role and addressing
    • Data mapping
    • Communication option cards
    • Programming software
    • Firmware compatibility
    • Licensing requirements
    • Project or parameter migration

A replacement component may support the same protocol but still require changes to network configuration or controller programming.

Physical and Environmental Fit

Review:

    • Mounting style and footprint
    • Terminal and connector orientation
    • Panel cutout
    • Cable clearance
    • Operating temperature
    • Humidity and condensation limits
    • Ingress-protection or enclosure rating
    • Shock and vibration rating
    • Washdown, dust, oil, or corrosive exposure
    • Hazardous-location approvals

A replacement that fits electrically may still require panel modifications or fail prematurely if it is not rated for the operating environment.

Safety Requirements

Safety relays, light curtains, interlocks, emergency-stop devices, and safety controllers require a separate application review.

Do not replace a safety-related component based only on voltage, dimensions, or terminal count. Confirm the intended safety function, safety rating, response time, output type, reset behavior, certifications, and validation requirements.

Safety-related changes should be reviewed and validated by qualified personnel under applicable standards and site procedures.

Step 4: Document and Test the Replacement

Before energizing a replacement, investigate whether an external condition contributed to the original failure.

Check for:

    • Incorrect or unstable supply voltage
    • Loose or overheated connections
    • Shorted wiring or loads
    • Ground faults
    • Excessive panel temperature
    • Failed fans or blocked cooling paths
    • Moisture, dust, oil, or contamination
    • Motor, encoder, or mechanical-load problems

Installing a replacement without correcting the cause of the original failure may result in another failure.

After installation, verify the wiring, configuration, communication, I/O operation, alarms, interlocks, direction of motion, and safe-state behavior before returning the machine to production.

Document:

    • Original and replacement part numbers
    • Series, revision, and firmware
    • Date and reason for replacement
    • Wiring or mounting changes
    • Software and configuration requirements
    • Backup-file location
    • Test and commissioning results

Update schematics, bills of materials, CMMS records, spare-parts lists, and approved-substitute lists as needed.

How Galco Helps with Obsolete Parts

Galco helps maintenance and engineering teams evaluate options for obsolete and hard-to-find industrial automation components.

Depending on the part and application, Galco can help identify:

    • Available exact replacements
    • Manufacturer-designated successors
    • Candidate cross-referenced alternatives
    • Send-in repair options
    • Retrofit or upgrade paths

Galco supports customers with technical product knowledge, cross-reference assistance, industrial component sourcing, and repair services for products including PLCs, VFDs, HMIs, servo controls, circuit boards, and power supplies.

Need help finding a replacement for an obsolete automation part?

Contact Galco with the manufacturer, complete part number, series or revision, and clear photos of the component nameplate. Call 800-575-5562 to discuss available replacement, sourcing, and repair options.

Frequently Asked Questions

What information is needed to cross-reference an obsolete automation part?

Start with the manufacturer, complete part number, series or revision, firmware, electrical ratings, installed options, and clear nameplate photos. Also provide information about how the component is used in the machine or control system.

Is a cross-referenced part always a direct replacement?

No. A cross-reference identifies a candidate replacement. Electrical, mechanical, communication, software, firmware, environmental, and safety requirements must still be verified.

Should an obsolete automation part be repaired or replaced?

Repair may make sense when the system is difficult to modify, a direct replacement is unavailable, or the component contains application-specific configuration. Replacement may be preferable when a verified exact unit or supported successor is available.

Can an obsolete PLC module be replaced with a newer version?

Sometimes. Compatibility depends on the PLC family, rack or chassis, processor, firmware, programming software, I/O configuration, terminal block, wiring, and communication requirements.