Industrial facilities often rely on automation components that have been in service for years. When a PLC module, variable frequency drive (VFD), HMI, sensor, relay, circuit board, or power supply becomes obsolete, finding the right replacement can quickly become a downtime issue.
To cross-reference an obsolete automation part, start by identifying the exact manufacturer, complete part number, series or revision, firmware, and installed options. Then compare the original component’s electrical, mechanical, communication, software, environmental, and application requirements against available replacement options.
The result may be an exact replacement, an updated manufacturer successor, a functional alternative, a repair, or a system upgrade.
A cross-reference should always be treated as a candidate replacement until compatibility is verified. Similar specifications or physical dimensions do not necessarily mean that two parts are interchangeable.
Industrial automation manufacturers regularly discontinue older product lines and introduce updated platforms. Even when a newer component appears similar, it may not support the existing hardware, software, wiring, or communication architecture.
For example:
That is why cross-referencing should be handled as a technical review, not simply a part-number search.
Before requesting a cross-reference, gather as much information as possible about the original component.
Useful details include:
Pay close attention to prefixes and suffixes. A small difference in a catalog number may identify a different voltage, enclosure, communication interface, feedback option, coating, or I/O configuration.
Original documentation can also help. Review schematics, wiring diagrams, bills of materials, maintenance records, equipment manuals, PLC programs, HMI applications, and drive parameter files when available.
Before removing a component that still powers up, back up any available configuration data. This may include PLC logic, HMI applications, VFD parameters, servo settings, network addresses, recipes, or safety-controller projects.
Once the original part and its application are understood, determine which replacement path makes the most sense.
An exact replacement uses the same complete part number, with the required series, revision, firmware, and options verified.
This is often the lowest-change option, but the same base model number does not always mean that two units are equivalent.
A manufacturer successor is an updated product identified by the original manufacturer as the replacement or migration path.
A successor may still require adapters, software conversion, parameter migration, new terminal blocks, or wiring changes. Always review the manufacturer’s migration documentation.
A functional alternative is a different product line or manufacturer that may perform the same required function.
This option may require additional engineering, rewiring, reprogramming, network changes, or renewed application testing. Similar ratings alone do not establish compatibility.
Repair may be practical when the machine is difficult to modify, the component contains application-specific configuration, or replacement inventory is limited.
PLCs, VFDs, HMIs, servo controls, circuit boards, and power supplies may be repairable depending on their condition and failure mode.
A retrofit modifies the machine or control system to use newer technology.
This may be the better long-term option when repair and replacement inventory are becoming unreliable or when multiple obsolete components create continuing lifecycle risk.
Before installing a replacement, confirm that it meets the complete application requirements.
Check:
For VFDs, compare the motor full-load current and required overload rating, not just horsepower.
Confirm that the replacement supports the required communication network or interface, such as EtherNet/IP, Modbus, PROFIBUS, PROFINET, DeviceNet, serial communication, or IO-Link.
Also verify:
A replacement component may support the same protocol but still require changes to network configuration or controller programming.
Review:
A replacement that fits electrically may still require panel modifications or fail prematurely if it is not rated for the operating environment.
Safety relays, light curtains, interlocks, emergency-stop devices, and safety controllers require a separate application review.
Do not replace a safety-related component based only on voltage, dimensions, or terminal count. Confirm the intended safety function, safety rating, response time, output type, reset behavior, certifications, and validation requirements.
Safety-related changes should be reviewed and validated by qualified personnel under applicable standards and site procedures.
Before energizing a replacement, investigate whether an external condition contributed to the original failure.
Check for:
Installing a replacement without correcting the cause of the original failure may result in another failure.
After installation, verify the wiring, configuration, communication, I/O operation, alarms, interlocks, direction of motion, and safe-state behavior before returning the machine to production.
Document:
Update schematics, bills of materials, CMMS records, spare-parts lists, and approved-substitute lists as needed.
Galco helps maintenance and engineering teams evaluate options for obsolete and hard-to-find industrial automation components.
Depending on the part and application, Galco can help identify:
Galco supports customers with technical product knowledge, cross-reference assistance, industrial component sourcing, and repair services for products including PLCs, VFDs, HMIs, servo controls, circuit boards, and power supplies.
Contact Galco with the manufacturer, complete part number, series or revision, and clear photos of the component nameplate. Call 800-575-5562 to discuss available replacement, sourcing, and repair options.
What information is needed to cross-reference an obsolete automation part?
Start with the manufacturer, complete part number, series or revision, firmware, electrical ratings, installed options, and clear nameplate photos. Also provide information about how the component is used in the machine or control system.
Is a cross-referenced part always a direct replacement?
No. A cross-reference identifies a candidate replacement. Electrical, mechanical, communication, software, firmware, environmental, and safety requirements must still be verified.
Should an obsolete automation part be repaired or replaced?
Repair may make sense when the system is difficult to modify, a direct replacement is unavailable, or the component contains application-specific configuration. Replacement may be preferable when a verified exact unit or supported successor is available.
Can an obsolete PLC module be replaced with a newer version?
Sometimes. Compatibility depends on the PLC family, rack or chassis, processor, firmware, programming software, I/O configuration, terminal block, wiring, and communication requirements.