Create or sign in to your account for the best pricing!

Your account pricing is now applied.

Toggle Nav
Search
My Cart

What is AC Power?

AC power, or alternating current power, is the type of electrical power that is used to power homes and businesses in most parts of the world. AC power is different from DC, or direct current, power in that it periodically changes direction.

The main advantage of AC power is that it is easier to transmit over long distances without losing energy. This is because the voltage of AC power can be easily adjusted using transformers. In contrast, the voltage of DC power cannot be easily changed, making it more difficult to transmit over long distances.

AC power is generated at power plants using generators that are driven by steam turbines or other means. The generators produce a continuous flow of electricity that alternates in direction at a specific frequency, typically 50 or 60 Hz (hertz). The frequency of the AC power is important because it determines the speed at which the power oscillates, which in turn affects the performance of electrical devices that use the power.

AC power is typically delivered to homes and businesses through power lines that are strung between poles or towers. The voltage of the AC power is typically high, typically around 115,000 volts, to reduce losses due to resistance as the power is transmitted over long distances. The voltage is then lowered to a safe level using transformers before it is distributed to homes and businesses.

In homes and businesses, AC power is used to power a wide range of electrical devices, including lights, appliances, and electronic devices. The AC power is typically delivered to the home or business through a service panel, which contains circuit breakers or fuses that protect the electrical system from overloading.

In conclusion, AC power is the type of electrical power that is used to power most homes and businesses. It is generated at power plants and transmitted over long distances before being distributed to homes and businesses. AC power is easy to transmit over long distances because its voltage can be easily adjusted using transformers.