Terminal Blocks - Connection Terminal and Screw Terminal Definitions
Terminal Blocks
Terminal Blocks (also known as connection terminals or screw terminals) are modular, insulated sections that fasten two or more wires together and consist of an insulating frame and a clamping component. Often associated with DIN rails in either IEC or NEMA rating, their adjustability allows wiring to be centralized and makes it easier to manage complicated control circuits. Today's control wiring solutions are gradually becoming more and more complex as equipment is constrained to smaller and smaller spaces, and industry calls for more responsiveness and higher amounts of automation. Within the control board, these modular components are snapped firmly into place on a mounting rail.
When modifications in the circuit must be carried out, terminal blocks can be easily added or removed from the rail without interfering with other wire terminations. In addition to minimizing complexity of control wiring, the plastic frames of terminal blocks also protect against shorts and subsequently provide increased safety to installers and service crews.
Insulating Body
The insulating body houses the current carrying elements. The body insulates the wire termination to reduce heat produced when current traverses through the wires. It also supplies a base for the clamping system and other elements including switches and fuses. The body of the terminal block has specially constructed holes for easy access to the clamping screws. The body also has a mounting foot that allows the terminal block to be clipped on and off the mounting rail without experiencing deterioration. The space saving style of a typical modular block allows high-density circuits to fit in a standard control panel. A 5mm wide block can deliver up to 60 terminations per linear foot. Standard 6mm single level blocks produce up to 50 terminations per linear foot; double level blocks can manage up to 100 terminations per foot.
Mounting Block Construction
Mounting block bodies can be constructed from Polyamide 6.6, Melanie 150, or Ceramic.
- Polyamide 6.6 is a sturdy thermoplastic material, manufactureded to work under any atmosphere and remain elastic and fracture proof from -40 degrees Celsius to 105 degrees Celsius. This substance offers high insulation, tracking resistance and a high flammability score. The durability and ease of handling of this material makes it the most frequently used.
- Melanine 150 is a resin-based thermoset plastic with an organic filler. Despite the fact that it's a far more fragile material than Polyamide 6.6, Melanine provides a high level of resistance to heat radiation. It is highly recommended for purposes where the continuous running temperature is anywhere between 110 degrees Celsius and 140 degrees Celsius.
- Ceramic is an exceptionally rugged material that can be utilized in extremely high temperatures approaching 250 degrees Celsius. Ceramic blocks can also operate in industrial plants with excessive dust deposits and abnormally corrosive atmospheres.
Polyamide 6.6 is an elastic plastic with high impact strength, halogen-free and UV-resistant characteristics, good tropical and termite resistance, high chemical resistance and excellent
aging attributes.
Current Carrying Parts
IEC vs. NEMA Classified Terminal Blocks
Terminal blocks are categorized as DIN (IEC) or NEMA, depending on characteristics, that include panel mounting method, standards and approvals and design characteristics. DIN type rails are IEC terminal blocks, which originated in Europe. DIN describes the channel or rail that the terminal block is secured to. The design offers more terminations per linear foot, which satisfies industry demands to maximize the number of terminations in a control panel. IEC blocks are easier to attach, wire and mark than NEMA style blocks. Rails are offered in 15mm, 32mm and 35mm widths. DIN blocks are typically compatible between manufacturers because the rail is standard and can be fashioned to manage a wide assortment of applications.
Approximately 60 % of the terminal blocks used in the U.S. are DIN type. Most designers give preference to DIN type because they offer:
NEMA terminal blocks, referred to as American-style, contain self-lifting pressure plates, binder head screws or box lug connectors. They are more frequently used for heavy-duty operations. However, NEMA blocks consume more panel space and offer fewer terminations per linear foot. Also, rail sizes differ across manufacturers, limiting the user's choices.
- Space saving, small compact designs and more units per foot.
- A wide range of block types for design flexibility.
- A worldwide recognition.
NEMA terminal blocks are:
- Cost-effective for some applications.
- More options for high current applications.
- Open construction, which allows for easier wiring.
The International Electrotechnical Commission (IEC) is a non-profit,
non-governmental international standards organization for all
electrical technologies.
The National Electrical Manufacturers Association (NEMA)
provides a forum for the development of technical and
electrical standards. The NEMA headquarters is in
Washington, D.C.
Selecting the Right Terminal Block
Choosing the correct terminal block is straightforward. Just follow the steps below:
- Determine current, voltage and wire size (AWG) to be used for the individual wire runs in the control or power distribution application.
- Define any special space constraints imposed by the application
- Considering the first two steps, select the appropriate rated feed-through terminal types to satisfy the electrical and space requirements. Select block widths. Double to block level and wire size if necessary to meet space requirements.
- Determine how many blocks (number of Poles) are needed, whether any blocks need to be jumped and how the jumper connections should be made (which place).
- Select special function block (ground, disconnect, fuse, indicating types, switch) based upon application requirements.
- At the end of each terminal block assembly, wherever a change in terminal block size occurs or when a side of a terminal block is not used, specify as end plate. Unused sides of terminal blocks must not be left uncovered and exposed.
- Determine where isolation partitions are needed to provide visual separation or to contain creepage within the terminal assembly. To ensure safety, isolation partitions separate blocks with different amperage ratings or voltages to prevent current/voltage jumping from one to another. Partitions also indicate to maintenance crew or electricians that there may be a different voltage in each of the groupings of blocks.
- For rail mounted blocks, select the type of rail mounting. Calculate the length required by totaling the individual widths (thicknesses) of the terminal blocks, end plates, isolation partitions and end stops.
- Mark wire terminations using marking tags.
DIN Terminal Blocks, like the ones pictured above, refers
to the channel or rail that the terminal block mounts on.
Just mount the rail and snap on terminal blocks and other
components.
Terminal Block Video Overview